Try searching by key words, order- or product code or serial number e.g. “CM442” or “Technical information”
Enter at least 2 characters to start the search.

Every millimeter matters

How much oil is in the tank? In international trade, only calibrated measuring devices can deliver an acceptable answer. Calibration can be done laboriously on site or directly at the factory, as Endress+Hauser does with a unique calibration rig.

04.03.2025 Text: Robert HabiI
A Micropilot level sensor using radar measurement technology

Oil and gas surpass all other commodities in terms of the volume that gets moved around. Every day, some 90 million barrels (14.4 million tonnes) of crude oil and natural gas are extracted, filled, stored temporarily and transported onward around the world. “In large storage tanks, every incorrectly measured millimeter of fill level could make a difference of several thousand euros straightaway,” Daniel Hoy from Endress+Hauser Level+Pressure explains. That is why measuring devices on large oil tanks must be calibrated verifiably according to internationally recognized standards such as OIML R85 or API 3.1B.

There are two options for verifiable calibration: In the first and most frequent one, a verification officer stands on the tank and measures the fill level with a measuring tape. The results are compared to those from the level sensor installed on the tank. The maximum permissible discrepancy is four millimeters. Obtaining various benchmarks involves emptying or filling tanks – expensive procedures that often take several days. Customers can save all this time and effort by choosing the second option, factory calibration. This requires a complex calibration rig, like the one Endress+Hauser has developed at the competence center for level and pressure measurement in Maulburg. “We precisely calibrate every radar sensor ordered for tank gauging on the rig. With multiple measuring positions along its 50-meter length, that takes at most an hour and a half,” says Daniel Hoy. The calibration rig stands in an elaborate purpose-built room and is the only one worldwide able to calibrate radar level sensors for tanks and stilling wells to an NMI-certified standard. The devices are allowed to be out by no more than one millimeter, as stipulated by the generally accepted OIML R85 recommendation.

Key facts

50m

is the maximum calibration distance. Thus the rig covers many tank sizes.

Key facts

0.5 mm

within the measurement range of up to 50 meters is the maximum measurement discrepancy of the device under test after calibration.

Endress+Hauser built the rig in response to industry developments: In the USA and in Europe especially, space at ports is becoming scarcer and so their storage tanks are being built taller. Gas tanks 50 meters high are not unusual. The pictures below show a simplified birds-eye view of how factory calibration of the radar sensors works.

The instrument under test is a Micropilot level sensor using radar measurement technology. ©Endress+Hauser

The instrument under test is a Micropilot level sensor using radar measurement technology.

Radar waves beam out into free space and some hit the reflector. ©Endress+Hauser

Radar waves beam out into free space and some hit the reflector, from where they bounce back to the sensor on the measuring instrument. The distance between the sensor and the reflector is determined based on the signal’s time of flight.

The two-sided reflector runs on rails. ©Endress+Hauser

The two-sided reflector runs on rails. Placing it at various positions between the laser and the level sensor provides a series of measurements.

The laser measures the distance to the device under test. ©Endress+Hauser

The laser measures the distance to the device under test and to the reflector with micrometer precision. After calibration, the sum of those distances corresponds to the exact overall length of the rig. Thus, the laser is the high-precision reference for measuring the instrument under test.

Partitions made of special foam absorb stray radiation. ©Endress+Hauser

Partitions made of special foam absorb stray radiation, as it is primarily the straight beams that are to be measured.

Read more about similar topics:

Downloads

Explore additional resources

document icon
Company magazine 'changes' 2/2024
The art of stable supply chains
download icon Download