Essayez la recherche par mots-clés, réf. de commande / code produit ou numéro de série, p. ex. "CM442" ou "Information technique"
Entrez au moins 2 caractères pour démarrer la recherche.
  • Historique

Endress+Hauser acquires SensAction

Concentration measurement technology bolsters flow portfolio

Date de publication: 14.03.2017

SensAction will operate as a division of the Endress+Hauser center of competence for flow measurement technology headquartered in Reinach, Switzerland. “This innovative technology is an excellent fit with our modern flow measurement portfolio,” says Dr Bernd-Josef Schäfer, Managing Director of Endress+Hauser Flowtec AG. “It allows us to further expand our range of products for measuring quality parameters.”

Already, Coriolis flow measurement devices from Endress+Hauser can determine not only mass flow, but density as well. Electromagnetic instruments are capable of measuring conductivity parallel to the volume flow. “These physical analysis parameters create direct value-add for the customer,” emphasizes Bernd-Josef Schäfer.

Endress+Hauser plans to integrate the SensAction instruments into its own program and open up new markets via the Group’s international sales structures. In addition, plans are in place to eventually combine the technology direct with Endress+Hauser flow instruments.

Innovative technology

The systems from SensAction measure the concentration of liquids with the help of surface acoustic waves, which are high frequency sound waves whose behavior can be compared to seismic waves created by earthquakes.

By analyzing the transmission time and amplitude, the acoustic parameters of the liquid, such as sound wave velocity, impedance and density, can be measured in order to quickly and precisely determine the concentration. Because they contain no moving parts, the systems are maintenance-free and do not suffer from wear-and-tear.

Apart from developing and manufacturing concentration measurement systems, SensAction also offers supplementary services, such as software products that rely on a laboratory measurement to provide a high degree of accuracy and user-friendliness for the customers’ applications. The key fields of application for the SensAction instruments include concentration measurements for liquid process media.

The acquisition of SensAction will be effective retroactively from 1 January 2017. Both parties have agreed to not disclose the details of the transaction. Stefan Rothballer and Michael Münch, two of SensAction’s founders, will continue to manage the innovative company’s business.

Téléchargements

    Endress_Hauser_SensAction_14-03-2017.zip

Liste de presse

Recevez les prochains communiqués de presse et actualités directement dans votre boîte mail. Restez à l'ordre du jour en vous inscrivant à la liste de presse Endress+Hauser.

Liste de presse Endress+Hauser

Endress+Hauser envoie régulièrement des communiqués de presse sur des sujets d'actualité et des informations sur l'entreprise aux professionnels des médias.

Sélectionnez les sujets qui vous intéressent : *
Sélectionnez les secteurs qui vous intéressent :

Voulez-vous recevoir des invitations aux événements presse (numériques ou en direct) d'Endress+Hauser ?

Informations personnelles

Les champs marqués d'un * doivent être remplis. Vous recevrez un e-mail de confirmation de votre inscription et le lien Internet correspondant. Vos données ne seront utilisées que pour la personnalisation de vos newsletters et ne seront pas transmises à des tiers. Les informations fournies le sont volontairement. Pour des raisons statistiques, nous effectuerons un suivi anonyme des liens.

Contact