Entrez au moins 2 caractères pour démarrer la recherche.
  • Historique

Electromagnetic Flow Fundamentals

FC104 - Two day (16 hours)

This Electromagnetic flow course provides maintenance/engineering personnel with an understanding of the principles of operation, focusing on concepts required to properly install and commission electromagnetic flow meters. We will also demonstrate how to properly troubleshoot & diagnose, test and repair common errors which may arise with this flow meter technology. This class consists of classroom/hands-on training with table top/live devices installed on our Process Training Unit (PTU).

PTU ©Endress+Hauser

Contenu

  • Electromagnetic flow meter technology basics / Electromagnetic flow meter overview

  • Proper installation and process influences on the measurement

  • Gathering data needed for commissioning

  • Sizing and verifying meter suitability for application / Field tooling

  • Meter commissioning / Meter verification

  • Possible sources of error and troubleshooting

  • Spare part identification and device repair

Objectifs

  • Explain the basic concepts of how an Electromagnetic flow meter operates

  • Understand what information is needed to properly configure the device

  • Install and commission Electromagnetic flow meters

  • Troubleshoot errors with Electromagnetic flow meters to determine the source of the issue and repair the device when needed

Qui devrait participer ?

  • Operations and maintenance personnel responsible for the installation, commissioning or maintenance of Electromagnetic flow meters.

Prérequis

Basic computer and instrumentation knowledge