Groupe Endress+Hauser

Médias

Événements

Votre carrière avec Endress+Hauser

Outils en ligne

Information Contact

E-direct Shop

Economique et direct : un rapport performances - prix inégalé sur une sélection d'appareils Endress+Hauser livrés rapidement et commandés facilement

E-direct Shop
Avoid false starts! Start-Up with Endress+Hauser...

Avoid false starts!

Start-Up with Endress+Hauser...

Our customers choose Endress+Hauser Start-Up safe in the knowledge that their devices are protected with an additional year’s warranty that includes complimentary commissioning within the first 6 months!

With demands on their engineering and maintenance personnel higher than ever, relying on Endress+Hauser service engineers makes sense. We’re experts in delivering a thorough job in the minimum possible time. It's what we do, time and again.

Avantages

  • Guaranteed peace of mind.

  • Cost-effective use of expertise and resources.

  • Includes free commissioning or device integrity check as required.

You’re in safe hands

Extended warranty is provided so you can rest easy, knowing your product is protected. As part of the Start-Up, you can also have your device commissioned by a qualified Endress+Hauser engineer at no additional cost!

If you choose to commission yourself, we offer a device integrity check within the first six months to ensure everything is running as it should. You’ll also receive a certificate detailing those instruments benefiting from the additional warranty.

Terms and conditions

  • Start-Up must be chosen at time of placing your order for new devices.

  • Start-Up will be invoiced with the new device and is party to similar payment conditions.

  • If a service tech is sent to a customer site within the first 6 months and the issue is deemed to be unrelated to warranty, the visit will be classed as a standard visit and charged as such.

  • If commissioning of the new device is needed, it is the customer’s responsibility to supply a commissioning date so that the visit can be planned.

Offer applies to mainland Canada only

  • All other countries, please refer to your local sales office for commissioning and warranty information.

  • Start-Up services are only available during normal working hours (Monday-Friday).

Contact

Endress+Hauser Canada Ltd
1075 Sutton Drive Burlington , Ontario L7L 5Z8 , Canada
Tél.: +1-905-681-9292
Tél.: +1-800-668-3199
Fax: +1-905-681-9444
Envoyer e-mail www.ca.endress.com